Other Parts Discussed in Thread: LM5160
Tool/software:
Hi,
I'm using the LM5160A module in a functional test board. Sporadically I'm struggling with defects on the IC. Local overheating always occurs at the same position in the chip. I cannot explain why this happens.
What I can measure:
LM5160A shows DIE burnout. There is an internal short between VIN - SW - PGND. The short is also measured from VIN to TP (thermal pad). The LM5160A works well for a long time. The temperature is also within range. But sometimes it happens that the IC gets a short. We tried short-circuiting the 12V output for a long time (24 h) -> no problem for the design. Also shorting the input voltage, which leads to excessive current in the body diode of the high side mosfet, does not damage the IC. The temperature under full load conditions looks well.
Now I'm at the point where I can't get any more insight into the IC.
Who can help me? Thanks!