Other Parts Discussed in Thread: LM5190
Tool/software:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello Muzammil
1. No, LM5190 provides two MOSFET drivers. You don't need to use gate driver ICs
2. No need to worry. LM5190 provides adaptive deadtime function.
3. Typically, it is okay to use down to 2mΩ sense resistor.
4. Yes, CC mode regulation target is controlled by the ISET pin voltage
5. Yes, if we assume the inductor current = the load current. IMON current is proportional with inductor current.

6. Yes, if VOUT is greater than VBIAS-TH

-EL
2. We have observed shoot through in Mosfets having Ciss 5nF. Mosfets with higher continuous drain current usually has high Ciss and ours is a high current application as well. Will this cause any problems ? How to tackle this it so there is not shoot through?
Hello Muzammil
-EL