This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25756: Operation with System Load but no battery

Part Number: BQ25756
Other Parts Discussed in Thread: BQ25750, BQ25751

Tool/software:

Hi,

This question is similar to "e2e.ti.com/.../bq25756-driving-the-system-when-the-battery-is-absent", I don't see an answer to that question, so I am asking here.

We plan to use this part in our product both with and without external 13.8Lead-Acid or LiFePO4 battery. The battery will be optional depending on the user's application. Our product can draw peak current to up to 3.5A, and may draw as low as 100mA during start-up. Typical current draw is 300mA at 13.8V.

Is this part suitable for operation without any battery? Our requirement would be that the converter supplies 13.8V with current varying between 100mA and 3.5A with no battery attached.

Thanks,