Other Parts Discussed in Thread: BQ25756
Tool/software:
Hi,
I am using the battery charger BQ2750. The datasheet says that if during powering the system load, the input voltage turns-off abruptly, the output transistor turns-on immediately (by BATDRV signal) to allow the battery to replace the external power driving the load.
But unfortunately I found that there is huge delay between the input drop to the output On - about 55 millisecond.
The result is that this mechanism works OK only for very light load, but I am using 10A load!. And not only that the system voltage drops long time before the output turn-on, but also the BATDRV signal can't startup to turn-on the MOSFET.
So, I wonder if there is a way to shorten the delay to less than 1millisecond?
If it is not possible, what is the best way to solve the problem?
Thanks,