Other Parts Discussed in Thread: USB2ANY
Tool/software:
Dear TI team,
My charger is in a 4s configuration. I have double-checked the 17.4k/0.1% ohm resistor on the PROG pin. I have also connected the 4.7uF capacitor to the PMID pin. My issue is that when powering up the board without a battery, the VSYS(min) register sets itself to 3.25V, and voltages at the VSYS pin start fluctuating from 9-13V. The voltages at the VBAT pin also fluctuate with random voltage values. The stat pin starts blinking, and the inductor creates weird noises. The CHG_Flag_Int and VBAT_OVP_Int starts blinking. As shown in this figure, these registers are causing the issue. Even if I correct these, these are set automatically.
I am unsure why this issue is present. When I connect the battery, the charger works fine when setting up the registers.
I am looking forward to hearing back.
Regards,
Ahmed Ali