This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25713: We were unable to successfully charge the battery.

Part Number: BQ25713


Tool/software:

Hello,

We are working on BQ25713 to charge 1S battery(18650 2800mAh Li-on 8C). We've filled registers below; 

1) BQ25713_REG_CHARGE_CURRENT - Value: 0x0580 (1408mA)

2) BQ25713_REG_MAX_CHARGE_VOLTAGE Value: 0x1068 (4200mV)

3) BQ25713_REG_INPUT_VOLTAGE Value: 0x0680 (5056mV)

4) BQ25713_REG_MIN_SYSTEM_VOLTAGE Value: 0x0D00 (3328mV)

5) BQ25713_REG_IIN_HOST Value: 0x0C80 (3200mA)

6) BQ25713_REG_IIN_DPM Value: 0x09C4 (2500mA)

7) BQ25713_REG_CHARGE_OPTION_0_EN_LWPWR // Disable

8) BQ25713_REG_CHARGE_OPTION_2_EN_EXTILIM // Disable

9) BQ25713_REG_CHARGE_OPTION_0_CHRG_INHIBIT // Disable

10) BQ25713_REG_PROCHOT_OPTION_1 Value: 0x00FF (255)

We were unable to successfully charge the battery. Is there a missing register that needs to be filled in or wrong filled register?

CHARGE_OK is HIGH

Best Regards,

Volk