This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1044: for 3 Meter cable USB3.1 gen1/dp 1.2 alt mode solution

Part Number: TUSB1044

Tool/software:

 Hi, Support Team

Q1: do we have TUSB1044 reference design is for Type-C to Type-C for 3 Meter cable USB3.1 Gen1/DP1.2 Alt mode?

Q2: according to attached file as format provide firmware program?

by the way, do we have USB3.2 cable E-MARK for PD controller solution?

if any suggestion, Please advise me.

Thanks,

Best regards,

Lawrence

  • Hi Lawrence,

    1. We have our TUSB1044 EVM that uses a Type-C plug on one side and a Type-C receptacle on the other. Its possible to use this with a 3 meter USB3.1Gen1/DP1.2 Alt mode USB-C cable if the cable loss is within the USB-C spec.

    2. Please refer to our TUSB1044 I2C mode control and tuning app note for a good reference on how to configure the 1044 over I2C. This should help with firmware development that needs to interface with the TUSB1044.

    do we have USB3.2 cable E-MARK for PD controller solution?

    We do not have e-marker solutions. I recommend asking the PD controller team if they know any.

    Best,

    Shane