Tool/software:
I am looking at the BQ25798EVM manual.
If I want to perform a simulation according to this manual, should I connect an electronic load in constant voltage mode to the J5 terminal?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I am looking at the BQ25798EVM manual.
If I want to perform a simulation according to this manual, should I connect an electronic load in constant voltage mode to the J5 terminal?
Hi Kenji,
Ideally, a sourcemeter or bipolar (4 quadrant) power supply in parallel with a large capacitor better simulates a real battery. If you only have an e-load in constant voltage mode, then I recommend placing a power supply in parallel to provide a base line voltage (like 2.6V*#of cells). Then set the e-load constant voltage setting to a higher voltage = battery voltage to be simulated.
Regards,
Jeff
Thank you for your reply.
I would like to simulate a 3.3V 4-cell battery.
Does this mean that I just need to connect in parallel to the J5 terminal an electronic load set to 13.2V constant voltage mode and a stabilized power supply set to an output of 13.2V?
Hi Kenji,
An electronic load in CV mode only clamps its voltage. Depending on its response time, the eload and charger output may oscillate. I recommend adding a >=1000uF cap in parallel with eload. Adding a parallel power supply to set a a minimum "battery" voltage is also recommended. The eload sinks current from the power supply until the charger output takes over.
Regards,
Jeff