Tool/software:
Hi,
We are developing a new product which uses two UCC27614 to drive each transistor in the MSCSM120DUM027AG. Our gate driver board had the wrong footprint for the UCC27614, so we turned it upside down and patched in the necessary pins. However, we only used one of the pins for VDD and one pin for GND. Could this be the cause of the broken driver?
Are the two GND and VDD pins bonded to the same die pad?
Setup:
Drive voltage +20 /-5V
Gate resistance: 3,3 ohm on, 3,3||3,3 ohm off.
Conditions at failure:
Bus voltage: 1V (one volt!)
Transistor peak current: 6A
Pulse width: 100us
Pulse frequency: 100Hz
Kind regards
Fredrik