Tool/software:
Hi Team,
Currently in my design, I measured a large ripple on the PoE input (800mV) and I want to reduce this ripple to below 500mV. Since my board space is not very large, I did not put a large capacitor at the input (on the design there is already a C94 capacitor with a value of 47uF/100V). I tried changing the value of the capacitors C248, C249 from 2.2uF/100V to 4.7uF/100V and I found that the ripple voltage decreased to only 540mV. So I want to ask:
1. Can I change the value of C248, C249 (see attached image) to reduce the input ripple voltage?
2. Do you have any better recommendations to reduce the ripple on this input?
Looking forward to hearing from you soon.
Thanks.