This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello Team,
I am using LM5163 in applicaion where we are having 12V input and 10V output with 0.4A Load. I have used Type 3 ripple circuit for this.
Below is the output ripple waveforms with CH2 is buck output (Red) and CH4 (green) is ripple at feedback
Without load :
With Load :
Is ripple waveform at feedback pin is ok with load condition? I have build this circuit on zero PCB board(without PCB layout).
Thank you.
BR,
Vaibhav
Hello Vaibhav,
If you have a breadboard that you built this circuit on, this is likely your issue. the waveform with load looks unstable. need to lay this circuit out on a PCB, with strict adherence to the layout guidelines, Additionally, please use the calculator spreadsheet to unsure satisfactory component selection to ensure stability.
Hope this helps,
David.