Other Parts Discussed in Thread: UCC28730, UCC28C53
Tool/software:
I'm trying to find a, preferably PSR, flyback converter that can handle
input from 15Vdc to 150Vdc
2 individually isolated outputs
and has a very low no-load consumption. I started looking at the UCC28730 which at first glance looks perfect but can not handle the low input voltage. Then I looked at the UCC28720 but from the forum I can understand that this is not suitable for multiple output flyback.
Does anyone have a suggestion to what is best to use?