Tool/software:
I have a system with several secondary windings, I'd like to reduce these 4 windings down to 2. We have one 24V rail which is the regulated rail. Then the other windings I would like to combine and tap off to produce my needed base voltages for post regulation.
With the UCC28740 I understand the need for the VS pin to monitor a secondary winding voltage directly.
I often see flybacks with designated aux windings for their own power supply. I cannot find a reason that this is mandatory. I would like to combine this aux winding into the tapped winding system and place the valley switching detection node on that winding. This won't affect the valley switching functionality at all will it? I can't see that it would, but didn't know if there was a relationship between Vdd & VS that I'm not realizing.
Primary : regulated secondary
Primary : unregulated multitap winding feeding flyback IC, gate drive & processor