Tool/software:
I'm following the AN2020 TI application note & making a template so as to predict the accurate IC temperature rise in our worst case scenario calculation. I've calculated the required rtja w.r.t copper, exposed pad & thermal vias seperately but I need a formula or technique which will combine all the rtja & give the final result.
I've attached the template with some rough calculation as per one of our board.
Also, I'm a bit confused on the following statement in the EIA/JESD51-1 standard: