This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25756: System Load in Parallel with Battery

Part Number: BQ25756

Tool/software:

Hi,

I plan on testing the BQ25756 in a system consisting of a battery pack (33.6V charging voltage, 2A charging current) that could be charged while it is connected to the system load. The system load could be turned off or on and draw up to 1A and operate at the same charging voltage. The battery pack has a built in battery management system.

Would there be any issues with the system load and battery sharing power from the BQ25756 charging output in the case that the system is turned on?

Thanks.