This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76907: Can the BQ76907 be connected to a 12.8V LiFePO4 battery module?

Part Number: BQ76907

Tool/software:

Hello
I am considering connecting the BQ76907 to a LiFePO4 battery module (12.8Vx2, 20000mAH).
Looking at the datasheet, it seems that the maximum measured voltage between each VC is about 5.5V.
In this case, is it possible to measure and balance the battery module?
If not, are there any equivalent products that can control the VCs at 12.8V or more?

  • Hi,

    The device's ADC is not able to measure more than ~6V/Cell. You would need to step down the voltage to the device's range using a resistor divider. Unfortunately, we don't have any devices in our portfolio that measure more than that. 

    Regards,

    Max Verboncoeur