This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27426: Fuel Gauge Configuration for 80% Charge Termination

Part Number: BQ27426

Tool/software:

I read the Quick Start Guide and TRM and learned that the taper rate allows bq27426 to synchronize with the battery’s charge termination point (i.e., the fully charged state).

If the product application consistently stops charging at 80% of battery capacity, will the bq27426’s fuel gauging function correctly, or are there additional recommended parameters that need to be configured?