This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC23525: Supports the IEC 60747-17 standard

Guru 12815 points
Part Number: UCC23525
Other Parts Discussed in Thread: UCC21551

Tool/software:

Hi,

Q1.
Please introduce a 2-channel isolated gate driver that meets the following conditions.
The conditions are that it can handle a current of about 4A and that it supports the IEC 60747-17 standard.

Q2.
Looking at the datasheet for the isolated gate driver, there are ICs that support the IEC 60747-17 standard and ICs that do not.
Does TI intend to support the IEC 60747-17 standard in the future?

Thanks,

Conor

  • Hi Conor,

    All of our gate driver datasheets will be updated to include the DIN EN IEC 60747-17 standard (VDE 0884-17). We are in the process of making the required edits to the datasheets. The previous standard was called DIN V VDE V 0884-10, so that is what you may see in datasheets for parts over a year old. 

    UCC21551 is a dual channel gate driver with a 4A output that may be of interest.

    Best regards,

    Sean