Other Parts Discussed in Thread: TPS23731
Tool/software:
Hi TI :
we would like to design 48V to 12V by 802.3bt PoE.
Could you help to provide reference EVB schematic for TPS23730 or TPS23731 ?
do you know what different TPS23730 and TPS23731 ??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Blue,
Thanks for reaching out!
In short TPS23730 is rated for 51W (Class-6) standard PD and TPS23731 is rated for 25.5W (Class-4) standard PD.
In majority of cases, BT PoE is for Class 5-8 (40W - 71.3W), and TPS23730 is recommended. Please see below pictures for more detailed information.
Best regards,
Diang