This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS562202: PSpice Simulation

Part Number: TPS562202


Tool/software:

Hi, 

Does this PSpice model work under non recommended values used on the inductor?
For example with my steady state simulation, 

Vout : 5V from Vin: 7.3V
Inductor used: 2.2uH, 140mOhms
Feedback voltage divider resistors: 68kOhms and 13kOhms
Output capacitors: 2 x 22uF + 1 x 0.1uF
Output load: 1A

I am trying to understand the effect of reducing the size of my inductors on the output ripple due for sizing reasons. 

Kind regards,

Richard