Other Parts Discussed in Thread: LM4041-N, REF50E, REF35
Tool/software:
For flux sensor mesuerements we want to use a Hall sensor where we need a constant current source of 2mA.
The manufacturer of the Hall sensor describes the circuit below for offset compensation. The sensor needs a constant current of 2mA.
Maybe you can give us some suggestions about the current source that can be used (e.g. LM4051?) and the instrumentation opamp and the output opamp shown in the circuit below? Or maybe a reference design with a hall sensor? We prefer a differential analog output for minimizing noise because it has to be connected with a measurement circuit (probably with a differential analog input but we have to select something for that).
The Hall sensor output is 200mV max (positive or negative) for the Hall sensor we are using. The output should be around 5V max I expect (depending on the controller/measuring system we are going to use but this is still under investigation)