This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLVM13640: Vout=12V characteristics shown for 6V max output part?

Part Number: TLVM13640
Other Parts Discussed in Thread: TLVM13660

Tool/software:

Hello, in www.ti.com/.../tlvm13640.pdf retrieved 10/28/2024 dated "April 2022", section 7.9 and specifically Figure 7-19 ("VOUT = 12 V, FSW = 2 MHz") show 12V output characteristics.

However, the part "VOUT1, VOUT2 to AGND, PGND" absolute maximum is listed as 6V.

Could you clarify why 12V operation is shown for this device as well as for TLVM13660? Is there a more updated version of this documentation?

Specifically, we would like to confirm that the other traces shown in the datasheet are from this device and not accidentally copied from other documentation.

Thank you.