Part Number: LM74900-Q1
Other Parts Discussed in Thread: LM74912-Q1, LM74912
Tool/software:
Dear Experts,
We are currently evaluating LM74900-Q1 and LM74912-Q1, with a maximum continuous current of 250A and a short-circuit protection current of 300A; I have some questions while reviewing the data manual and hope to receive answers;
1. What is the maximum current limiting value for LM74900-Q1 and can it meet our requirement of limiting current to 250A?Does RIlim have a range of values? What does 12 in the formula refer to?What is the basis for deriving this formula

2.What is the maximum value of short-circuit protection current and what is the maximum threshold for short-circuit protection? Does RISCP have a range of values? I saw that the maximum input voltage for ISCP to SC- is 0.3V. Does this mean that the maximum short-circuit protection current for a 1m Ω Rsense is only up to 300A? Vsns-scp up to 0.3V?


3. Can LM74900-Q1/LM74912 drive external 300A MOS?
Best Regards