This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-R2: Chemical ID

Part Number: BQ34Z100-R2
Other Parts Discussed in Thread: BQSTUDIO, GPCCHEM

Tool/software:

Hi expert

I found a cell with similar properties in bqstudio chemistry table, which cell is SK-E710.

I would like to inquire whether there is any problem in applying the ID of SK-E710 cell to SK-E556 cell product.

The SK-E556 cell has same cathod,anode chemistry and  OCV range with SK-E710 (id: 7547)

If possible, what is the max error limit?

 

<SK-E710 cell>

Chemistry : LiMn2O4 (Co,Ni)/carbon, 4.2V

ChemID : 7547
Nominal capacity : 68.9Ah

<SK-E556 cell>

Chemistry : LiMn2O4 (Co,Ni)/carbon, 4.2V

ChemID : ????
Nominal capacity : 55.6Ah

 Best regards.