This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD3138FW_LLC: UCD3138FW_LLC:Where should I add the DTC interrupt processing?

Part Number: UCD3138FW_LLC
Other Parts Discussed in Thread: UCD7138, UCD3138A, UCD3138

Tool/software:

Hi all,

I want to use the DTC function of the UCD7138, which is controlled by the UCD3138A, so I need to customize the UCD3138FW_LLC firmware.

I would like to add an interrupt process when the CIMINT_ALL_DTC occurs. However, I cannot figure out where I should add it. Should it be added to the fast_interrupt() function in the interrupts.c file?

And can I find the cause of CIMINT in any member of the Union or Struct?

I would greatly appreciate it if you have any sample code for CIMINT.

Best Regards,

YUKIOOYAMA