Other Parts Discussed in Thread: UCC28951
Tool/software:
Hello,
I am trying to design an isolated DC-DC converter with the following specifications:
- Vin: 16-90 Vdc
- Vout: 48 Vdc
- Iout max: 30A
Using the TI Webench Power Designer, I entered my input and obtained the schematic. I downloaded the simulation circuit and created the schematic as suggested by Webench. However, it is not working as expected. My output voltage changes when I adjust the load resistor.
Attached below are the simulation results . I have made all possible changes on my side in the simulation, but I am still not getting a constant output voltage regardless of the load changes.