Part Number: TPS23753A
Other Parts Discussed in Thread: TPS23730
Tool/software:
Hi team,
The following application note states that it is generally not a problem to hot plug an adapter with power on and excessive inrush current flowing through it.
https://www.ti.com/jp/lit/an/slva306a/slva306a.pdf
Why is this not a problem?
Also, in my experiment, an inrush current of 100A flowed.
The EVM diodes are rated at 50A and I am wondering if this could be a problem.
I would like to know if the “no issue” in the application note means that it will not break as a PoE IC, or if the diode is attached correctly, it will not be a problem.
Best Regards,
Ryu.