Other Parts Discussed in Thread: TPS2553,
Tool/software:
Dear Teams,
About TPS2553 and TPS25221.
In order to confirm that the OCP and OTP functions of the device work properly, if the overload is intentionally applied, the recommended operating range will be exceeded.
Our inspection specifications: 2.3A load and device enter thermal shutdown.
1. Will the device be stressed or damaged?
2. Is the overcurrent limiting function of the device 100% inspection?
Thank you.