This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS4H160-Q1: transient high current

Part Number: TPS4H160-Q1

Tool/software:

Hi Team,

May the TPS4H160-Q1 be able to withstand a high transient current of 15A per channel for approximately 10us?

The customer's output current under normal conditions is approximately 2A per channel, but there is a large transient current at the start-up moment. 

Thanks!

Regards,

Ivy

  • Hello Ivy, 

    The internal current limit is fixed at ICL(int). Tie the CL pin directly to the device GND for large-transient-current applications. that range is from 8-14A. Operating outside of this is not recommended and could damage the device. 

    BR, 

    Alan