Tool/software:
We are working on a project with BQ79631 and we would like to use the main ADC. The problem is: some information contradicts each other.
Let start with this: in this document SLUSEC2A, Page 8, "VSn, to AVSS, where n = 3 to 16" range min..max "3V..5V",
and "VSn - VSn-1, where n = 2 to 16" range min..max "-1V..5V".
In sluucc3: BQ79631EVM Evaluation Module Page 19. example: VC5 (pin VS5) is on the 5V (TSREF), and the VC6 (pin VS6) is connected trough a divider to Link Plus, so is max 5V+4V=9V.
The VC7 (pin VS7) is below the TSREF, what means VS7-VS6 = -4V.
That means, the VCC6 is above the 5V, and VS7-VS6 is below the -1V.
My question would be: what is the correct way to use the Channels of the BQ79631 Main (and also the AUX) ADC?