This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79652-Q1: Can you recommend an 18s BMS?

Part Number: BQ79652-Q1


Tool/software:

We are working on a hyperloop prototype. Initially, we selected a propulsion motor that required a 12s cell configuration and were using that integration. However, we have now decided to switch to the Hobbywing X11 Max motor, which requires an 18s cell configuration.

We want to design our own Battery Management System (BMS) and do not wish to purchase a pre-made BMS system. Furthermore, we prefer not to connect BQ EVMs in series.

Considering these factors, which BMS integration would be appropriate for powering this motor?