This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8868Z-Q1: LP8868Z-Q1 UVP Open circuit detection

Part Number: LP8868Z-Q1

Tool/software:

My purpose is to reserve the UVP pin float and still detect the LED open load and short circuit. Is it possible?

After I measured,When the UVP pin is in the float state, the Fault can still detect the LED open state, how is it done? Because the datasheet describes that when the VUVP < 1.2V for 100us, the LED open load will be detected.

I guess when the LED is open load , the Error Amplifer output high for 100us is mistaken for Switching FET open, then the Fault is pulled down.