Tool/software:
Hi,
The battery NTC is connected to the TS pin.
We want to add a buffer and use an ADC to ready the temperature from TS pin as well.
We found the REGEN (Pin 22) is not alway present. It is off when the battery provides power to the system and OTG is disabled.
Can we use 5V which generated from the SYS (Pin 15, 16) instead of REGN?