Other Parts Discussed in Thread: SN74AHCT541
Tool/software:
Hello,
I’m currently using a couple of UCC21750 to drive a 10kW half bridge IGBT converter.
Some time happen that some pulse was missing at the output of one of the two drivers. The first think that I’ve though was that pulse is missing on the input of the driver and with my surprise I’ve noted that the pulse at the input of the driver was truncated in amplitude at about 2.5V.
For each input of the driver there is a resistor of 5.6k and a capacitor of 100pF between driver input and GND.
The power supplies are good and stable in all conditions and no fault was come out from the driver.
As you can see in the image (the vertical scale is slightly different between them), the blue trace is the pulse before the resistor of 5.6K and the green trace is the pulse after that resistor (input of the driver). Looks like that sometime the impedance of the driver input goes low than 55k pulldown.
Of course, I had tried to change some IC driver but the issue persists.

Do you have any idea what can cause this behaviour?