Other Parts Discussed in Thread: TPS61287
Tool/software:
Hi there,
I'm have a project that requires 25V and draws approx. 6 amps. I'd like to be able to use a single LiPo battery at 3.7 volts with a high discharge current (~40 amps). Packaging, however, is a consideration. Can anyone recommend a boost converter that can boost the voltage from 3.7 to approx. 25V while being able to handle a current of around 6 amps (slightly higher to be on the safe side) and is as small as possible? Thanks!
Regards,
Phil