This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7H5001-SP: Current Limit Threshold Typical Value

Part Number: TPS7H5001-SP

Tool/software:

Hello,

I notice in the datasheet for this part that the Electrical Characteristics table (7.5) lists the Current Limit Threshold as 1.05V (typical) & 1.09V (max).

But then in the Typical Characteristics plots (7.10, figures 7-17 & 7-18) the lowest threshold range over temperature and voltage is 1.0525 - 1.068V (with the 25C data being at the high end of that range). The prior listed typical value falls outside this range, which seems odd.

In using this part, with Vin=5V, I have measured the threshold to be about 1.065V, which appears to fall in line with the plots (approximately).

Is the 1.05V listing supposed to be the minimum value (instead of typical)?

Thanks
Chad