Other Parts Discussed in Thread: LM25185
Tool/software:
Hi there,
I'm design a flyback converter but I'm getting some trouble during PSpice simulation related to compensasion network.
The converter specs are presented below.
Vin: 20~36V, Vout:16V, Pout:42W, VD:0.7, NPS: 1:1, Lm=10uH, Cout:200u, D_Nom = 0.3736, R_Cs = 10mΩ
Compensation design results:
AM = 1.39
ACS = 10
WzRPH=640151.46
WzESR=1000000
Wp=2253.57
Calculating a Gain in cross-over frequency (F_Co = 1kHz)

Calculating RCOMP
RCOMP = 261kΩ
CCOMP = 0.85nF
CHF = 5.7pF
Simulating this circuit in PSPICE I got these currents in Lprimary (green) LSec (Red), it seams my compensation network is not working very well.

Am I doing something wrong during the compensation design?
Thank you