Part Number: TPS61288
Tool/software:
Hello.
This is Kwonjoon Lee from South Korea.
I would like to ask about TPS61288's discharging operation (triggered by the EN pin).
(Detailed Situation)
1. My TPS61288's output is connected to (a input of) TPS7A4901, and
my TPS61288's input voltage and target voltage are 4V and 16V, respectively.
2. I have a plan to disable TPS61288 by pulling down the EN pin to 0V before turning off the VIN of TPS61288.
(It seems that TPS61288's discharging operation triggered by the EN pin is not modeled in the SPICE model of TPS61288)
(Questions)
1. I would like to ask if TPS61288's output voltage is rapidly decreased to the input voltage (4V) of TPS61288
when the EN is pulled down to 0V (what is a falling time?).
2. I would like to ask if TPS61288's output voltage is completely turned off (to 0V)
when the input voltage of TPS61288 is pulled down to 0V (what is a falling time?).
Best regards,
Kwonjoon Lee