Tool/software:
Hello to all.
I've been trying to design a battery powered LED design circuit. I am using TPS61235 for boosting a 18650 battery paralelled with 2 cells. The LED board consumes 1.3A. I also use BQ29700 for battery protection. Battery voltage goes straight to the boost converter, enables and boosts after waiting necessary time for boost converters precharge. Then the 5.1V powers the circuit. And the MCU gives PWM to the gate/base of the semiconductor switching element. When this happens there is a heared noise coming out from the circuit and the input voltage starts to bounce.
I increased the frequency of the PWM to 100kHz from 1kHz and the audible noise is lost but even if the frequency is high the input bounces still. This yields the minimum input voltage level of the boost converter not satisfied or battery protection cuts the connection and the LEDs start to work uncontinuously. This happens around the voltage of the battery reduces to around 3.2 - 3.1V. There is still 240mV pk-pk according to the oscilloscope. I tried to add an 1uH inductor and capacitor just before the switching element comes in. (Same inductor with boosting). Nothing changed.
My original scenario was when the battery is discharged to 2.8V the battery protection cuts the battery connection from the circuit and waiting for recharge. In this case I can control the operation with software not by the hardware. I cut the PWM operation in around 3.3V which results insufficient battery capacity usage.
First i tried to design a darlington pair but didn't satisfied. Then replaced FZT with CSD17575Q3 and removed R14,R17,Q9 and shorted NBASEJ with NBASE.
When the load current increases more unstable the circuit gets. So the uncontinuous phase can start even in 3.7V - 3.9V of the battery.
I tried the load by connecting it to the output of the boost converter everything worked fine even in 2A loads etc the problem occurs only in switching phase.
Any help is highly appreciated