This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC23513: UCC23513 working on 200kHz switching frequency for LLC

Part Number: UCC23513
Other Parts Discussed in Thread: UCC23525

Tool/software:

The datasheet only test the frequency at 20kHz. It seems only support low switching frequency IGBT. 

May I know whether can support 200kHz for LLC MosFET driver?

BR,

Gary

  • Hi Gary,

    The UCC23513 can switch at almost 25MHz unloaded.

    The package has a power rating of 0.75W, operating junction temperature of 150C and a Theta JA of 126°C/W, which means that if the ambient temperature is 125°C, UCC23513 can cycle a 1nF capacitor load at 18V at 600kHz before its thermal rating is exceeded at this temperature extreme. 

    (150-125)/126 = 0.2W

    CV^2 = (1nF) * (18V)^2 = 324nW

    f_sw = 0.2/ 324n = 612kHz

    However, it is usually more important to determine the switching losses of the Mosfet. This will vary based on the gate driver's output drive strength and the externally added Rg and Cgs. If the switching losses are too high, the Mosfet will burn up at a much lower frequency than the gate driver. 

    For example, C3M0015065D is a SiC FET with a nominal 1.5mJ turn-on and a 0.7mJ turn off. However, this will change based on externally added Rg and Cgs. 

    The UCC23513 has a pretty good output drive strength compared to competitors, and it can help to improve switching efficiency of mosfets and enable higher switching frequencies. In the measurements below, you can see the UCC23525 can provide higher output drive strength when the externally added Rg is less than 12 Ohms:

    C3M0015065D with UCC23513: Eon with 50A and 5 Ohm Rg

    Eon vs. Id, Rg=5 ohms, Cgs=0nF

    50A Eon vs. Rg

    Best regards,

    Sean