Tool/software:
Hi,
I use the reference LM317MQDCYR (SOT223 package). A 135mA load must be supplied during 100ms.
Is existed a transient thermal impedance coefficient as power MOSFET? Or can we consider only the thermal resistance specified in the datasheet?
The thermal impedance is about 60°C/W
The drop voltage is about 10V.
Maximal junction temperature is 134°C for 125°C specified for 55°C ambiant temperature.
is it ok for a short duration or is it forbiden?
thanks for your help,
Best regards,