This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24650: Designing a Solar Harvesting Power Supply with Battery Storage Capabilities

Part Number: BQ24650

Tool/software:

Hello,

I am current designing a solar power supply with a 12V 2W solar panel to charge a 6V 6Ah Lithium Battery.

I am considering to use the BQ24650, however I was wondering if there are similar PMUs I could use that can be simulated in Pspice or Psim?

Also, with the given input voltage and power to the PMU, would this work for this PMU?