This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM317L-N:Resistor R2 not installed

Part Number: LM317L-N

Tool/software:

I am using a Japanese translation software.
Thank you for your question.

I am using resistors R1 = 240Ω and R2 = 2kΩ (resistor connected between the adj terminal and GND) so that the input voltage is 15V and the output voltage is 12V.

Question 1) R2 was unintentionally left uninstalled. Will this damage the LM317LZ/NOPB?

Question 2) With R2 not installed, the output is about 13.5V. Will the output voltage become unstable if R2 is not installed?