Part Number: TPS61161
Other Parts Discussed in Thread: TPS61160,
Tool/software:
Hi,
I was going to include a schematic but there seem to be no way to attach any file or image? If I click on insert Insert -> Image/video/file the only thing you can add is a link? How bizarre and absurd is that? Am I missing something?
About this post, some questions about the TPS61161 and TPS61160. I need to make sure that the brightness is 100% when the system boots (i.e. before the micro can control the CTRL pin).
1. How do I configure the hardware to ensure that is so? Do I just place a pull-up on the CTRL pin to 5V? Does that ensure that Vfb value is set to a specific value by default? If so, is such value 200mV?
2.the dimming of the TPS61161 and TPS61160 be controlled exclusively from a digital pin from a 3V3 micro even if Vin is 5V correct?
3. Table 6.5 page 6 it says "CTRL pull down resistor" and it provides a value up to 1.6K. But the resistor is not shown or mentioned anywhere in the datasheet. And Figure 13 (and also the internal block diagram) shows there is no resistor. Which resistor is "CTRL pull down resistor" referring to? Is that mentioned because any pullup added externally on CTRL pin needs to be within a certain range perhaps?
4. dimming can be controlled exclusively with PWM on the CTRL pin instead of the 1-wire commands, correct?
5. If yes, why is there also the much more complex RC dimming on the FB pin as mentioned in "7.4.4 External PWM Dimming"? It seems to only take more components and no advantage...
Thank you