Tool/software:
Hi ti team,
Does the TPS2571 meet the following requirements and confirm the following critical test items?
1,USB 2.0 Electrical requires Test Mode (Test_Packet, Test_J, Test_K and Test_SE0_NAK), how to make DUT enter TEST mode?
If EH is USB3.1 Gen1, please also inquire whether there are special instructions or techniques to enter loopback or compliance mode before testing TX or RX.
(You can seek assistance from the Chipset Vendor and inquire about how to enter Test Mode.)
2,Does the DUT support Suspend / Resume? If so, please provide instructions on how to enter Suspend / Resume mode?
Does the DUT support Standby Mode? If so, does it support remote wake up?
3,Does the DUT support Low Speed Downstream Signal Quality?
4,Does the DUT support Battery Charging 1.2?
5,Does the DUT have an onboard Hub?
6,Does the DUT support an external Hub? If not, it must display the corresponding message or prompt.
(Test Item: 10.3.5 and 7.3.7 Hub Error Message Test)
7,If there is an external Hub for support (if there is no support for a Hub, you can skip this question), how many layers of Hub can the DUT connect to?
8,What types of devices does the embedded host support (e.g. pen tray, mouse... etc)?
How many types of devices can the DUT support (if the customer does not specify any device for testing, Allion can also recommend)?
9,Please fill in the product information (P1 to P5) at the beginning of the report (such as the attached document). If you don't know how to fill it out, please fill in the IA_VBUS_RATED item first (required). You can leave the rest blank for testing, but the testing time may be extended due to the additional time needed for verification.
10,If the Embedded Host requires special SOP for operation, please provide the operational procedures.