Part Number: TPS61235P
Tool/software:
Hello there,
I am trying to build a 18650 li ion battery powered LED lighting system, the LEDs consume 1.3A as a board. I used TPS61235P for boosting the input level and did my calculations on 5.1V fixed supply.
I use transistor low side switching topology in my circuit powered all by the boost converter. The output voltage level of the IC is 5.2V and when the load is connected it reduces to around 5.143V. It works okey in 3.3V-4.2V of the battery voltage but when it discharges to 3.2V it gets in probably pre-charge phase because then the LEDs blink in long off time period. I think the sensing topologies inside of the IC is affected due to abnormal operation of the IC. I tried to give the 5.1V from outside of the board and used boost converter for just supplying the MCU therefore switching the FET, it worked as expected. Without any problems. I shorted the CC pin to AGND but that is not the solution.
Overall as much as i increase the load current as soon as it behaves abnormally.
Then I checked the design;

It is aimed to get 3A output current


This is the top layer and the feedback pin is shorted to the output (5.1V)


Heres the mistake i've done I think because the feedback line is shorted to the output Polygon.
Could this be the reason of 5.2V output instead of 5.1V fixed? Thanks.
Regards,
Kaan