Other Parts Discussed in Thread: TPS61033EVM
Tool/software:
Hello,
I am using a TPS61033DRLR to boost an input voltage of 3V to 5V. I have connected the circuit as recommended by the datasheet however when I apply 3V to the input. Immediately the Input and Ground pins show as a short and it draws huge current from my DC power supply. Seems like the internal MOSFET at the SW and GND pin blows up. Need urgent help in this matter.

(Cin and Cout are both 10uF, 16V)
I have re-checked the connection multiple times and have blown up 3 ICs already.
Thanks,
Aleric.