Tool/software:
Hi
We are adapting BQ25620 IC in our design. We have RTC IC that consumes sub micro amp. The RTC is being powered directly from the battery which is also connected to BAT pin (so the battery V+ is connected to both RTC and BAT pin). When we switch BQ25620 to shipping mode, the current consumption is higher than expected for the RTC approx 325uA while it should be 600nA (including BQ25620 in shipping mode). We tried to switch to shutdown mode but still same behavior.
Is it ok to connect RTC IC prior to BAT pin? Could this be the issue? Appreciate any recommendation or suggestion