This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55288: TPS55288

Part Number: TPS55288
Other Parts Discussed in Thread: TPS55289

Tool/software:

Hi,

I would like to use this device to convert 24V input to 0-15.5V output and 0-3.5A output.
This device can only generate Vmin = 0.8V.  How do I get down to 0V and 0A output?

Thank you.
Luke

  • Hi Luke,

    As the datasheet described, the min recommended output voltage is 0.8V. The operation below Vout=0.8V is not guaranteed by TI.

    If you want to get 0V, you can write OE=0, and enable load discharge function to get 0V.

    BRs,

    Bryce

  • Hi Bryce,
    Thanks for your reply.
    I am evaluating this device for our power supply design.
    Do you have any reference design that is suitable for the following specs:

    Input voltage: 24V
    Output Voltage range: 0 - 15.5V
    Output current range: 0 - 3.5A (across voltage range).
    Digitally controlled by Microcontroller for Output Voltage and Output current.

    Thank you.

    Best regards,
    Luke

  • Hi Luke,

    From theoretically, it is hard to output such output voltage at 24Vin, the operation can't be guaranteed.

    TPS55289 is more suitable here except the 0V output voltage.

    BRs,

    Bryce