Other Parts Discussed in Thread: TPS25730EVM, TPS25730
Tool/software:
I am looking for a USB C PD SINK chip.
The purpose is to use it as a power supply for an audio amplifier.
There is no battery. Also, it is a priority to receive the maximum voltage from the PD SOURCE.
It would be nice if the program is as simple or absent as possible.
It would be nice if it can receive up to 100W of maximum power.
It would be nice if the circuit is simple.
Can this part TPS25750 be a good solution?